AnsweredAssumed Answered

make: *** No rule to make target

Question asked by Patrik Schantl on Oct 7, 2014
Latest reply on Oct 7, 2014 by Erwan Y
Hello,

currently I am trying to import and use an exported project within the SPC5Studio.

Several weeks ago, I have un-installed SPC5Studio after I made a backup of my projects because I had a problem with the hal libraries. In the mean time, there come several updates for the SPC5Studio which I installed.
After importing an old project, I can´t build them any more. I am always getting following warnings/errors:

15:10:45 **** Build of configuration Default for project E14003_FunktionsmusterV2_SPC560D_test ****

make -j4 all

Makefile:134: C:/SPC5Studio/eclipse/plugins/com.st.tools.spc5.components.platform.spc560dxx_1.0.0.201408011351/component/lib/rsc/rules.mk: No such file or directory

make: *** No rule to make target `C:/SPC5Studio/eclipse/plugins/com.st.tools.spc5.components.platform.spc560dxx_1.0.0.201408011351/component/lib/rsc/rules.mk'. Stop.

I understand, that the folders do not exist because they are from the old SPC5Studio installation. But how can I use the project in the new installation?
I do not want to clean the SPC5 application because I have changed several parts of the low level drivers which shouldn`t get lost.

Best regards,
Patrik

Outcomes