AnsweredAssumed Answered

M24SR04 EEPROM direct access

Question asked by mereu.daniele.001 on Feb 24, 2016
Latest reply on Mar 2, 2016 by JP Miller
Hi all,
I'm using a M24SR memory connected by I2C bus to a Freescale M0 microcontroller.
Given that the free space for the firmware is very little, I have problems integrating the ST library for reading and writing access to the NDEF files.
So, I was wondering if it was possible to access the EEPROM memory directly without using the ISO-DEP protocol, but accessing to the locations of the EEPROM memory with standard I2C command.
In my firmware I only have to access to a NDEF text file for reading and read the first 10 bytes of this file.
So I ask you:
       
  1. Can I access in reading mode to any location of the EEPROM memory bypassing the state machine of the device?
  2.    
  3. If yes, how can I find the starting address of the file that I previously wrote?

Thank you all in advance
Daniele

Outcomes