AnsweredAssumed Answered

L6470 motor power interlock

Question asked by basso.fred on Feb 11, 2014
Latest reply on Feb 17, 2014 by Enrico Poli
I am using an L6470 controller in an application that requires an interlock circuit to stop motor rotation if the interlock switch opens. Is it possible to safely switch 24V power to the VSA and VSB pins off then on to remove and re-apply motor power. Is it safe to allow the CP to run while VS is turned off?

Outcomes