AnsweredAssumed Answered

fatal error: opening dependency file

Question asked by ViRuS2k on Sep 13, 2014
Latest reply on Sep 15, 2014 by Erwan Y
Hi,

I have tried to compile an example with the SPC5Studio Wizard and get the following errors:

20:36:34 **** Incremental Build of configuration Default for project ChibiOS-RT SPC56ELxx Test Application for DiscoveryPlus ****
make -j4 all
      0 [main] sh 1656 sync_with_child: child 3980(0x188) died before initialization with status code 0xC0000142
     14 [main] sh 1656 sync_with_child: *** child state waiting for longjmp
/bin/sh: fork: Resource temporarily unavailable
Compiling boot.s
Compiling crt0.s
Compiling ivor.s
Compiling vectors.s
C:/SPC5Studio/eclipse/plugins/com.st.tools.spc5.components.platform.spc56elxx_1.0.0.201409031447/component/lib/src/boot.s:26:0: fatal error: opening dependency file .dep/boot.o.d: No such file or directory
compilation terminated.
make: *** [build/obj/boot.o] Error 1
make: *** Waiting for unfinished jobs....
C:/SPC5Studio/eclipse/plugins/com.st.tools.spc5.components.platform.spc56elxx_1.0.0.201409031447/component/lib/src/crt0.s:1:0: fatal error: opening dependency file .dep/crt0.o.d: No such file or directory
C:/SPC5Studio/eclipse/plugins/org.chibios.spc5.components.kernel.port.gcc.spc56elxx_2.6.4.201409031447/component/lib/src/ivor.s:42:0: fatal error: opening dependency file .dep/ivor.o.d: No such file or directory
compilation terminated.
C:/SPC5Studio/eclipse/plugins/org.chibios.spc5.components.kernel.port.gcc.spc56elxx_2.6.4.201409031447/component/lib/src/vectors.s:1:0: fatal error: opening dependency file .dep/vectors.o.d: No such file or directory
compilation terminated.
compilation terminated.
make: *** [build/obj/ivor.o] Error 1
make: *** [build/obj/crt0.o] Error 1
make: *** [build/obj/vectors.o] Error 1

20:36:35 Build Finished (took 810ms)

The files are avaliabe in the directories.

OS: Windows 8.1, 64bit

very frustrating ;(

Outcomes