AnsweredAssumed Answered

IAR + STM32VLDISCOVERY won't flash MCU

Question asked by fratrik.milan on Oct 11, 2010
Latest reply on Oct 12, 2010 by fratrik.milan
Hi,
i have a problem with this evalution board. I opened the project in EWARM 5.50 and tried to Download & Debug the base project(with blinking diodes), but i get this error message
Failed to load flash loader ..../FlashSTM32F100xB.flash
The debugging session could not be started. Either the debugger initialisation failed or the output file ..../DISCOVER.out was corrupted.

in the debug log window is
Loaded macro file: C:\IAR Systems\Embedded Workbench 5.4_2\arm\config\flashloader\ST\FlashSTM32F10xxx.mac
Failed to load flash loader: C:\IAR Systems\Embedded Workbench 5.4_2\arm\config\flashloader\ST\FlashSTM32F100xB.out
Failed to load flash loader: C:\IAR Systems\Embedded Workbench 5.4_2\arm\config\flashloader\ST\FlashSTM32F100xB.flash


Debugging without downloading works.
Can somebody help me pls?

Outcomes