AnsweredAssumed Answered

Can USB OTG lib. support two FS USB PHY for STM32F205 ?

Question asked by cakali.anil on Mar 12, 2014
Latest reply on Mar 13, 2014 by Clive One
I am going to use STM32F205 series MCU in my project, because it has two FS USB PHY. I am going to use one PHY as host, another PHY as device. Can USB On-The-Go host and device library(UM1021) support two FS USB PHY simultaneously? If the answer is yes, how can i configure dual FS PHY pins for  USB On-The-Go host and device library?

Thanks.

Outcomes