AnsweredAssumed Answered

[Bug] CubeMX generates wrong ETH_PHY_ADDRESS for the Nucleo-144 F7

Question asked by cnoviello on Jan 21, 2016
Latest reply on Feb 26, 2016 by Mosnier.Alain
Hi,
I want just to signal that CubeMX generates a wrong ETH_PHY_ADDRESS inside the stm32f7xx_hal_conf.h file when a project for the Nucleo-144-F7 is generated. The address is declared as equal to 1:

...
#define DP83848_PHY_ADDRESS             0x01
...

while it should be equal to 0x0 as clearly stated inside the Nucleo-144-F7 documentation. This causes that the code inside the low_level_init() function is wrong.

Outcomes