AnsweredAssumed Answered

how to set up OpenOCD in eclipse

Question asked by hobb.epy on Jan 10, 2016
Latest reply on Jan 11, 2016 by tarekb
Hi,
I need help to install openOCD with eclipse.
i have install eclipse and gcc compiler. it is compiling also. but i tried to set up openOCD and got some errors. Error as following.

Open On-Chip Debugger 0.9.0 (2015-05-19-12:06)
Licensed under GNU GPL v2
For bug reports, read
embedded:startup.tcl:60: Error: Can't find openocd.cfg
in procedure 'script'
at file "embedded:startup.tcl", line 60
Error: Debug Adapter has to be specified, see "interface" command
embedded:startup.tcl:60: Error:
in procedure 'script'
at file "embedded:startup.tcl", line 60


plz help me this. I m using nucleo103RB. 

Outcomes