AnsweredAssumed Answered

Installing ST-LINK/V2 USB drivers.

Question asked by b.m.002 on Jan 8, 2016
Latest reply on Jan 9, 2016 by b.m.002
Hi, I'm a newbie, and I have just started working with STM32 and the GNU tools available, and can anybody explain what is correct from the following quote on how to install
which is on ( http://gnuarmeclipse.github.io/openocd/install/ )

OpenOcd:

ST-LINK/V2

One example of compatible drivers are the ST-LINK/V2 USB drivers, from ST, available as part number STSW-LINK009. Download the stsw-link009.zip archive, extract its content to a separate folder, and run the dpinst_amd64.exe (or dpinst_x86.exe) with administrative privileges.


I Have two versions of OpenOCD
ST-LINK_USB_V2_1_Driver
and
ST-LINK_USB_V2_Driver

Has anyone done it this way before?

Thanks.

Outcomes