AnsweredAssumed Answered

USB Driver issues

Question asked by fox.matthew on Jun 10, 2013
Latest reply on Jun 10, 2013 by fox.matthew
In the user manual for the discovery board, it says that an installation wizard should appear when I connect the board to my computer for the first time, but that didn't happen.  I downloaded the driver from here: http://www.st.com/web/catalog/tools/FM146/CL1984/SC724/SS1677/PF251168

When I went to try to run some of the example programs (I'm using Keil), I had errors of the wrong file names for the drivers.  So I went into the file (C:/Keil/ARM/STLink/) and the file that the debugger was looking for -  ST-LINKIII-KEIL.dll - wasn't there, but there was a file named - ST-LINKIII-KEIL_SWO.dll.  I renamed the second one to the one it was looking for to see if that would fix the problem, but now I am getting an error "No ST-LINK detected."  
Any idea on what I'm doing wrong, or a way to make this work?  Thanks for the help!

Outcomes