AnsweredAssumed Answered

STEVAL-IDW001V1 documentation?

Question asked by neff.vance on Apr 28, 2014
Latest reply on Nov 20, 2014 by Gerardo Gallucci
Hi,

I just received a STEVAL-IDW001V1 eval module.  It is meant to connect to a Discovery F0 board, but intend on using it with a STM32F215 processor based device.  I haven't found much documentation about this eval board.  I have:

STEVAL-IDW001V1 - Wi-Fi daughterboard for STM32F0DISCOVERY
which includes a schematic and a general outline of what the board can do.  No specifics as to what the jumpers are for, what the important connections are, etc.

STEVAL-IDW001V1 Schematic diagram
This seems to have no relation to the eval board???

SPWF01Sx - Serial-to-Wi-Fi b/g/n intelligent modules
This does, at least, give pin-out for the WiFi module being evaluated alond with some min/max ratings.

And, the most useful so far:
SPWF01Sx AT Command set reference guide

Is there any detailed info on the eval board, or is this it?

Thanks for any additional info!
Vance




Outcomes