AnsweredAssumed Answered

iNemo STEVAL-MKI062V2 using C++

Question asked by fauria.oriol on Dec 2, 2010
Latest reply on Feb 22, 2011 by beffumo.fabio
Hello everyone,

I've just purchased an evaluation board (iNemo STEVAL-MKI062V2) and I'm trying to run an application in Visual Studio 2010 Professional in C++. Here are my doubts:

- As user guide I just found the pdf (Application Note AN3144) but I've realised that this is for the Version1 (STEVAL-MKI062V1). Is there any difference between V1 and V2?

- Then, I've tried to use the help manual for version 1 and create a program. But I can't connect the board.

in the line:
          
iNEMO_Return = INEMO_SDK_ConnectFunction("PL_001:COM12, BD115200");

the iNEMO_Return variable, returns me an 8 (which means CMD_TIMEOUT)
Then, Visual studio says:

iNEMO_SDK.dll', Cannot find or open the PDB file
PL_001.dll', Cannot find or open the PDB file

even though I have both files in the Project folder

Any idea to solve this? Cause by now I couldn't connect.
I have to say that the iNEMO application works fine.

Thanks in advance.

Oriol

Outcomes