AnsweredAssumed Answered

Matlab Embedded Coder Build Error

Question asked by joshi.shailesh on Dec 26, 2015
Latest reply on Dec 27, 2015 by joshi.shailesh
While trying to build a simple LED simulink model using embedded coder I get the following error in last few lines of diagnosis report:
"C:/MATLAB/SupportPackages/R2015a/armcortexm/toolbox/target/supportpackages/arm_cortex_m/cmsis_rtos_rtx/src/cmsis_rtos_init.c"
In file included from C:/MATLAB/SupportPackages/R2015a/STM32F4-Discovery_FW_V1.1.0/Libraries/CMSIS/ST/STM32F4xx/Include/stm32f4xx.h:245:0, 
                 from :0: 
C:/MATLAB/CMSIS-SP-00300-r4p5-00rel0/CMSIS/Include/core_cm4.h:151:0: warning: "__FPU_USED" redefined [enabled by default] 
       #define __FPU_USED       1U 
 ^ 
:0:0: note: this is the location of the previous definition
In file included from C:/MATLAB/SupportPackages/R2015a/armcortexm/toolbox/target/supportpackages/arm_cortex_m/cmsis_rtos_rtx/src/cmsis_rtos_init.c:8:0: 
C:/MATLAB/SupportPackages/R2015a/armcortexm/toolbox/target/supportpackages/arm_cortex_m/cmsis_rtos_rtx/include/mw_cmsis_rtos.h:6:22: fatal error: cmsis_os.h: No such file or directory 
 #include "cmsis_os.h" 
                      ^ 
compilation terminated. 
gmake: *** [cmsis_rtos_init.o] Error 1
C:\Users\Shail\Documents\MATLAB\stm32f4discovery_gettingstarted_ert_rtw>echo The make command returned an error of 2  
The make command returned an error of 2 
 
C:\Users\Shail\Documents\MATLAB\stm32f4discovery_gettingstarted_ert_rtw>An_error_occurred_during_the_call_to_make 
'An_error_occurred_during_the_call_to_make' is not recognized as an internal or external command, 
operable program or batch file.
Please help me with this

Outcomes