AnsweredAssumed Answered

LD8 (over-current) blinking

Question asked by martinu.jiri on Jun 3, 2013
Latest reply on Jun 3, 2013 by martinu.jiri
Hi all,

on my discovery STM32F4 the LD8 is blinking and I don't know why. There is nothing connected to 3V nor 5V pins but some 6 ADC inputs 5 PWM outputs, one UART and one I2C data connections. All devices are powered from an external supply and all grounds are connected together (including the Discovery board ground). The board is powered from external 5V power supply connected to the 5V pin on the Discovery board. Everything is working fine only the LD8 blinks...

I have measured the 3V output from the board and it looks like OK.

I really don't see the reason why it is blinking...

Don't you have any idea what to check or what could be the reason of LD8 blinking?

Thank you in advance...

Outcomes