AnsweredAssumed Answered

USB HID STM32F4Discovery 64 bytes

Question asked by diakov.alex on May 27, 2013
Latest reply on Jun 4, 2013 by chizhovich.dmitry
Hello,

It's the first time that I use the USB protocol. I want to connect my PC to the STM32 microcontroller via the USB HID.
I've seen example of HID from STM. I need to transmit and to receive data. Right now I can transmit and receive only 2 bytes. How I can do it with 64 bytes?
 I want to find a basic example (for STM32F4Discovery) that explains this communication in details.
I understand that this problem isn't very difficult. Unfortunately, I have no idea how I can solve it. 



Thank you.

Outcomes