AnsweredAssumed Answered

Newcomer to STM32F429I-Disco, exceed program limit problem

Question asked by sterevo on Nov 29, 2015
Latest reply on Nov 30, 2015 by Clive One
Hello,

I'm trying to build a demo program (from firmware package) for STM32F429I - disco and i can't even rebuild the program due to the limit exceeding error. I'm confused here. Am i wrong with using Keil-MDK for this program? Because I can't even think that a firmware program will be rejected by the IDE. It works fine with STM32F4-disco firmware though. 

Any suggestion from the masters?

I'm using keil MDK-ARM with these software information. 

IDE-Version:
µVision V5.15
Copyright (C) 2015 ARM Ltd and ARM Germany GmbH. All rights reserved.


License Information:
Bagas Prima
ITB
LIC=----


Tool Version Numbers:
Toolchain:        MDK-Lite  Version: 5.15.0
Toolchain Path:    C:\Keil_v5\ARM\ARMCC\Bin
C Compiler:         Armcc.exe        V5.05 update 2 (build 169)
Assembler:          Armasm.exe        V5.05 update 2 (build 169)
Linker/Locator:     ArmLink.exe        V5.05 update 2 (build 169)
Library Manager:    ArmAr.exe        V5.05 update 2 (build 169)
Hex Converter:      FromElf.exe        V5.05 update 2 (build 169)
CPU DLL:               SARMCM3.DLL          V5.15.0
Dialog DLL:         DCM.DLL              V1.13.2.0
Target DLL:             STLink\ST-LINKIII-KEIL_SWO.dll      V2.0.15.0_KEIL
Dialog DLL:         TCM.DLL              V1.14.5.0

Outcomes