AnsweredAssumed Answered

STM32 HAL Libs I2S 16bit Stereo?

Question asked by Hess.Marco on Nov 25, 2015
Latest reply on Nov 29, 2015 by helin.mikko.001
I am confused with the HAL I2S libraries as there does not seem to be support for 16bit stereo (2 channels).

I admit, I am a bit new on I2S but I suspect that with 44100 sampling frequency with two channels of 16 bits each, I need to transfer 32bits per stereo sample to the codec.

The HAL Libraries don't seem to support that. The only modes are the following:

#define I2S_DATAFORMAT_16B               ((uint32_t)0x00000000)
#define I2S_DATAFORMAT_16B_EXTENDED      ((uint32_t)0x00000001)
#define I2S_DATAFORMAT_24B               ((uint32_t)0x00000003)
#define I2S_DATAFORMAT_32B               ((uint32_t)0x00000005)

With the DATAFORMAT value providing bits for two fields on the chip:

In the reference manual 28.5.8 SPI_I2S configuration register (SPI_I2SCFGR)
I find there are two fields related to this: 

Bits 2:1 DATLEN: Data length to be transferred with values for 16, 24, and 32 bits.

and

Bit 0 CHLEN: Channel length (number of bits per audio channel) with 9 for 16 bit and 1 for 32 bits

In the the DATAFORMAT values in the HAL Libraries there is no #define for
transfer of 32bits with 16bit channels. i.e.  ((uint32_t)0x00000004)

What am I missing?

On the same issue, using DMA I suspect I need to do a 32bit memory to 2*16 SPI type transfer to get this right.


Outcomes