AnsweredAssumed Answered

high frequency PWM

Question asked by contreras.alexander on Apr 24, 2013
Latest reply on Apr 25, 2013 by contreras.alexander
Hi, want to generate a 24MHZ 50%DC PWM, I have follow this example ,but I can't get more than 500Khz, please help me.

void TIM_Config(void)
{
/* -----------------------------------------------------------------------
    TIM3 Configuration: generate 4 PWM signals with 4 different duty cycles.

    In this example TIM3 input clock (TIM3CLK) is set to 2 * APB1 clock (PCLK1),
    since APB1 prescaler is different from 1.
      TIM3CLK = 2 * PCLK1
      PCLK1 = HCLK / 4
      => TIM3CLK = HCLK / 2 = SystemCoreClock /2

    To get TIM3 counter clock at 28 MHz, the prescaler is computed as follows:
       Prescaler = (TIM3CLK / TIM3 counter clock) - 1
       Prescaler = ((SystemCoreClock /2) /28 MHz) - 1

    To get TIM3 output clock at 30 KHz, the period (ARR)) is computed as follows:
       ARR = (TIM3 counter clock / TIM3 output clock) - 1
           = 665

    TIM3 Channel1 duty cycle = (TIM3_CCR1/ TIM3_ARR)* 100 = 50%
    TIM3 Channel2 duty cycle = (TIM3_CCR2/ TIM3_ARR)* 100 = 37.5%
    TIM3 Channel3 duty cycle = (TIM3_CCR3/ TIM3_ARR)* 100 = 25%
    TIM3 Channel4 duty cycle = (TIM3_CCR4/ TIM3_ARR)* 100 = 12.5%

    Note:
     SystemCoreClock variable holds HCLK frequency and is defined in system_stm32f4xx.c file.
     Each time the core clock (HCLK) changes, user had to call SystemCoreClockUpdate()
     function to update SystemCoreClock variable value. Otherwise, any configuration
     based on this variable will be incorrect.
  ----------------------------------------------------------------------- */

  GPIO_InitTypeDef GPIO_InitStructure;

  /* TIM3 clock enable */
  RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE);

  /* GPIOC and GPIOB clock enable */
  RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC | RCC_AHB1Periph_GPIOB, ENABLE);

  /* GPIOC Configuration: TIM3 CH1 (PC6) and TIM3 CH2 (PC7) */
  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7 ;
  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ;
  GPIO_Init(GPIOC, &GPIO_InitStructure);

  /* GPIOB Configuration:  TIM3 CH3 (PB0) and TIM3 CH4 (PB1) */
  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1;
  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ;
  GPIO_Init(GPIOB, &GPIO_InitStructure);

  /* Connect TIM3 pins to AF2 */
  GPIO_PinAFConfig(GPIOC, GPIO_PinSource6, GPIO_AF_TIM3);
  GPIO_PinAFConfig(GPIOC, GPIO_PinSource7, GPIO_AF_TIM3);
  GPIO_PinAFConfig(GPIOB, GPIO_PinSource0, GPIO_AF_TIM3);
  GPIO_PinAFConfig(GPIOB, GPIO_PinSource1, GPIO_AF_TIM3);
}

void PWM_Setup(void)
{
    /* Compute the prescaler value */
  PrescalerValue = (uint16_t) ((SystemCoreClock /2) / 28000000) - 1;

  /* Time base configuration */
  TIM_TimeBaseStructure.TIM_Period = 665;
  TIM_TimeBaseStructure.TIM_Prescaler = PrescalerValue;
  TIM_TimeBaseStructure.TIM_ClockDivision = 0;
  TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

  TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure);

  /* PWM1 Mode configuration: Channel1 */
  TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
  TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
  TIM_OCInitStructure.TIM_Pulse = CCR1_Val;
  TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;

  TIM_OC1Init(TIM3, &TIM_OCInitStructure);

  TIM_OC1PreloadConfig(TIM3, TIM_OCPreload_Enable);

  /* PWM1 Mode configuration: Channel2 */
  TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
  TIM_OCInitStructure.TIM_Pulse = CCR2_Val;

  TIM_OC2Init(TIM3, &TIM_OCInitStructure);

  TIM_OC2PreloadConfig(TIM3, TIM_OCPreload_Enable);

  /* PWM1 Mode configuration: Channel3 */
  TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
  TIM_OCInitStructure.TIM_Pulse = CCR3_Val;

  TIM_OC3Init(TIM3, &TIM_OCInitStructure);

  TIM_OC3PreloadConfig(TIM3, TIM_OCPreload_Enable);

  /* PWM1 Mode configuration: Channel4 */
  TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
  TIM_OCInitStructure.TIM_Pulse = CCR4_Val;

  TIM_OC4Init(TIM3, &TIM_OCInitStructure);

  TIM_OC4PreloadConfig(TIM3, TIM_OCPreload_Enable);

  TIM_ARRPreloadConfig(TIM3, ENABLE);

  /* TIM3 enable counter */
  TIM_Cmd(TIM3, ENABLE);
}

thx in advance

Outcomes