AnsweredAssumed Answered

Ideas for improvement STM32CubeMX

Question asked by Charles on Nov 20, 2015
Latest reply on Nov 27, 2015 by anne
1. Timer Configuration
Add thetimerconfigurationcalculatorwhich ofthe requested Interupt Time or Frequency calculate Counter Period (ARR) and conversely the input values shows the parameters counter. Excellent would be a graphical display of output PWM etc.
2. Timer Configuration
Now we see Clock Source: Internal clock Why not see currently set value of Internal Clock?
3. Graphical highlighting functional groups of pins
For example, When scroll over UART in list Pinout they might highlight pins occupied this Peripheral . If the periphery of the conflict highlight graphically what pin.
This is important especially if you are using STM32Cube simultaneously with the  hardware (PCB) design.

Outcomes