AnsweredAssumed Answered

ST-LINK/V2 Commandline - HALT does't work

Question asked by mueller.wolfgang on Apr 19, 2013
Latest reply on Feb 28, 2014 by goff.steven
Hi,
for an automatic test, i need to Halt and Run a STM32.
It works without problems with the STM32 ST-LINK Utility, but not (program is  still running) when I use the CLI (st-link_cli.exe) in this way:

st-link_cli.exe -c SWD -Halt

the answer for this statement is:
STM32 ST-LINK CLI v1.5.1
STM32 ST-LINK Command Line Interface

Connected via SWD.
Connexion mode : Normal.
ST-LINK Firmware version : V2J17S4
Device ID:0x416
Device family :STM32L1xx medium density


All other statements give a message that the statment were accepted

Can anyone check this, maybe with older firmware?
What tool can I use alternativly?

Thanks in advance
Wolfgang

Outcomes