AnsweredAssumed Answered

M24SR - mistake in table 67 Datasheet

Question asked by saban.eyal on Feb 4, 2014
Latest reply on Feb 10, 2014 by ST NFC
hi , 
1.i have been playing with M24SR16-Y for few days , just  want to inform that there is a     mistake in table 67 .
  the Payload written in table 67  :   00 A4 00 07 02 D2 76 00 00 85 01 01
  should Be                                   :   00 A4 04 00 07 D2 76 00 00 85 01 01 00 (According                                                    to Chapter 5.6.3 , also checked with the IC return 90 00.)
the CRC  matched to the Correct Payload (including the PCB  byte = 0x02 Or 0x03)


Outcomes