AnsweredAssumed Answered

ADC Port Issues

Question asked by cozzens.brian on Mar 30, 2013
Latest reply on Oct 7, 2014 by jeevananthan.luxsumi
So I am having an interesting issue with configuring the ADC to work with anything but PortA.  I can hook it to any pin on port A, change the ADC channel, and it will work.  However, I have tried doing the same on PortB and PortC, but it doesn't seem to work.  I enable the PortB/C clock, configure the pins on those ports appropriately, but still nothing.  Here is my configuration code:

void ADC_Configuration(void)
{
  ADC_InitTypeDef ADC_InitStructure;
  DMA_InitTypeDef DMA_InitStructure;
  GPIO_InitTypeDef GPIO_InitStructure;


  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE);
  RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1 | RCC_APB2Periph_GPIA | RCC_APB2Periph_AFIO, ENABLE);


  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3;
  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN;
  GPIO_Init(GPIOA, &GPIO_InitStructure);




     
  /* DMA channel1 configuration ----------------------------------------------*/
  DMA_DeInit(DMA1_Channel1);
  DMA_InitStructure.DMA_PeripheralBaseAddr = ADC1_DR_Address;
  DMA_InitStructure.DMA_MemoryBaseAddr = (u32)&ADC_ConvertedValue;
  DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC;
  DMA_InitStructure.DMA_BufferSize = 1;
  DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
  DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Disable;
  DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;
  DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
  DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
  DMA_InitStructure.DMA_Priority = DMA_Priority_High;
  DMA_InitStructure.DMA_M2M = DMA_M2M_Disable;
  DMA_Init(DMA1_Channel1, &DMA_InitStructure);
  
  /* Enable DMA1 channel1 */
  DMA_Cmd(DMA1_Channel1, ENABLE);
    
  /* ADC1 configuration ------------------------------------------------------*/
  ADC_InitStructure.ADC_Mode = ADC_Mode_Independent;
  ADC_InitStructure.ADC_ScanConvMode = ENABLE;
  ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;
  ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_None;
  ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
  ADC_InitStructure.ADC_NbrOfChannel = 1;
  ADC_Init(ADC1, &ADC_InitStructure);


  /* ADC1 regular channel6 configuration */ 
  ADC_RegularChannelConfig(ADC1, ADC_Channel_3, 1, ADC_SampleTime_55Cycles5);


  /* Enable ADC1 DMA */
  ADC_DMACmd(ADC1, ENABLE);
  
  /* Enable ADC1 */
  ADC_Cmd(ADC1, ENABLE);


  /* Enable ADC1 reset calibaration register */   
  ADC_ResetCalibration(ADC1);
  /* Check the end of ADC1 reset calibration register */
  while(ADC_GetResetCalibrationStatus(ADC1));


  /* Start ADC1 calibaration */
  ADC_StartCalibration(ADC1);
  /* Check the end of ADC1 calibration */
  while(ADC_GetCalibrationStatus(ADC1));
     
  /* Start ADC1 Software Conversion */ 
  ADC_SoftwareStartConvCmd(ADC1, ENABLE);
}

Outcomes