AnsweredAssumed Answered

Flash STM32F103 via SPI

Question asked by hieber.jan on Oct 9, 2015
Latest reply on Oct 9, 2015 by qwer.asdf
Hi,
i have an application with an STM32F103 and a Raspberry Pi, connected via full duplex SPI.

I want to implement automated flashing of the STM. The idea is:
RPi contacts STM32 via SPI and if STM32 does not answer or has an old version of my software,
I want to flash the STM over SPI with the RPi.

I could connect the BOOT Pins and Reset to the RPi and get the STM into a bootloader.

Can I flash the STM32 with the default bootloader via SPI?

Background: Users should be able to use a factory new STM without knowledge about the hardware or even electronics.

Outcomes