AnsweredAssumed Answered

USB CDC Driver

Question asked by najmee.taha on Feb 25, 2013
Latest reply on Feb 26, 2013 by Clive One
Hello,

Can someone inform me whether I can use (or do I need) USB CDC Driver on Windows CE. I am planning to connect STM32F4 Discovery to Cuwin Touch Screen panel which is operated on Windows CE.

I checked the 'readme' file which comes with the driver and it says it is only compatible with Windows 98 SE, 2000, XP, Vista, 7.

Thanks for the help

Outcomes