AnsweredAssumed Answered

ST-LINK V2 Virtual Machine speed

Question asked by jayaraman.ram on Feb 5, 2013
Latest reply on Feb 6, 2013 by Clive One
Hi All,

I am using Keil uVision 4 with the ST-Link in the STM32L Discovery board. I can load a 150K binary on my windows machine in less than a minute but on my virtual machine it takes close to 4 minutes!

The virtual machine is running on a macbook pro with beefy specs [ 2GHz Quad i7 with 12GB RAM , 4Gb for the VM and a SSD hard drive ] . I know the specs dont matter as much for the transfer speed but I cannot figure out why the performance would be so different.

I am flashing using SWD [ not JTAG ] not sure if that makes a diff either.

Any help here is appreciated!

Thanks

Outcomes