AnsweredAssumed Answered

CubeMX 4.9 and USB host + fatfs

Question asked by k.alex on Aug 21, 2015
Latest reply on Oct 27, 2015 by astirfreak
Hello!
I apologize for my bad English, but I do not have anyone to ask.
My task is to create a USB host to work with flash pametyu. I also use fatfs.
I'm using a microcontroller STM32f407VG. To create a project I use CubeMX 4.9. Just to study, I use the example of FatFs_USBDiskSTM32Cube_FW_F4_V1.6.0.
What is the proper question.
Analyzing the example I knew how to work with flash memory, but after creating the project using CubeMX I could not do anything himself. Can anyone suggest how to write code after the creation of the project in order to be able to mount a drive to create a file and write to it anything.
Thanks in advance.

Outcomes