AnsweredAssumed Answered

STM32F10x StdPeriph SPI DMA ?

Question asked by H.Rick on Aug 16, 2015
Latest reply on Aug 18, 2015 by H.Rick
Guys,

I want  to try the example from :
STM32F10x_StdPeriph_Lib_V3.5.0\Project\STM32F10x_StdPeriph_Examples\SPI\DMA

and I follow from readme.txt

par How to use it ?

In order to make the program work, you must do the following :
 - Copy all source files from this example folder to the template folder under
   Project\STM32F10x_StdPeriph_Template
 - Open your preferred toolchain
 - Rebuild all files and load your image into target memory
 - Run the example

but I get this error on
MDK-ARM :


stm32f10x_rcc.c: Error:  #5: cannot open source input file "..\..\..\Libraries\STM32F10x_StdPeriph_Driver\src\stm32f10x_rcc.c": No such file or directory

From which directory can I get that ?

Which main.c will I use ? from the SPI_DMA directory or from "user" directory ?

Thanks

Outcomes