AnsweredAssumed Answered

STM32CubeMX freezes when generating code

Question asked by jansen.neil on Aug 11, 2015
Latest reply on Aug 21, 2015 by 68516
Hi,

STMCubeMX is freezing every time I try to generate code for an STM32F429 project.  This is my first time using it, but everything so far has been pretty straightforward, and I haven't given it any crazy parameters that would seem unreasonable.

The exact steps to reproduce the problem are: Load the IOC file (pasted below).  Click Project -> Generate Code.  It will display a progress bar, and will basically stay there forever (hours, etc).  I've tried it several times, and it does the same thing every time.

I will try re-generating the project and trying that, but figured I'd post this here to see if anyone else has had the problem, and to see if anyone here could re-create the problem.  

Here's my 'STMF429ZETx.ioc' file:
http://pastebin.com/8hR9gveS

And an image of the app, in its frozen state:
http://imgur.com/pOawxyl

Oh, my OS platform is Windows 8 on a pretty standard Lenovo laptop.  My Java JRE version is 8.0.51.16.

Any help would be appreciated.

Thanks!

Outcomes