AnsweredAssumed Answered

USB Host example on STM32F7 (or STM32Fx) without class-driver?

Question asked by nikolaou.christos on Aug 10, 2015
                                                               
           
Hi,

            Is             there any USB host example without class-specific driver? I see some             examples in the Cube lib, but all are class-specific eg HID/MSC/etc

            I would like to have a 'direct' comms between a F7-disco and an external USB device via plain usb endpoints.
            So, I have to see how to communicate from a host application to the external device via usb pipes/endpoints.

            Is there something that I can have as an example project for that?

            Regards
            Christos
           
blank.gif
                                               

Outcomes