User Activity

i am planning to build an dpoae device so which one do u prefer STM32MP157D-DK1 processor or STM32H7A3 microcontroller is enough?  for STM32MP157D-DK1 can u suggest some videos on how to use it ,the ide for it how to access the GPIOS .u can also sugg...
how to connect sine wave generation code to the TouchGFX interface and when a button is clicked it has to move to second page and trigger the generation ,how to use the mvp model,this the code for the sine wave generation and contiously writing to da...
will this code work? #include <gui/screen3_screen/Screen3View.hpp> //#include <math.h> #define PI 3.1415926 // Declare the DAC handle (assuming it's defined in another file) extern DAC_HandleTypeDef hdac1; static bool generateSineWave = false;...
can you please suggest me a best stm32processor board which has adc and dac and usb port, ethernet wifi which uses stm32cube ide