User Activity

Any idea to open the MX and see how clock is setup?This project was created on TrueSTUDIO as reported in the error message (old_MX_IDE.jpg).  Hit CONTINUE or MIGRATE give same error message (continue.jpg).Seem it says needing MX 5.3.0 and FW_F1 V1.8....
https://github.com/leechwort/u8g2-stm32-example/tree/masterAny advises on opening this?  I brought the needed Hardware Nucleo F401RE.  However the latest IDE and MX are not able to read the project.What is the general advises and procedure to port be...
Further to this earlier post, any chance now is a BMA400 SPI library already ported to STM32CubeIDE?Many thanks
From RM0461, Reference manual, STM32WLEx advanced Arm®-based 32-bit MCUswith sub-GHz radio solutionIs it correct that there are TWO RTCs inside STM32WLE5JCI6TRa) one is the normal STM32 RTC and just call RTC in many ST application notesb) the other i...
There are quite a number of cell chemistry for Lithium (and possibly others).  Which one is good for Lora:Transmit time of 1.5 seconds or less, current 1C or less. Recharge 0.5C to be safe (may be 1C on spec.).Normal (non transmit) low duty cycle loa...