User Activity

Further to this earlier post, any chance now is a BMA400 SPI library already ported to STM32CubeIDE?Many thanks
From RM0461, Reference manual, STM32WLEx advanced Arm®-based 32-bit MCUswith sub-GHz radio solutionIs it correct that there are TWO RTCs inside STM32WLE5JCI6TRa) one is the normal STM32 RTC and just call RTC in many ST application notesb) the other i...
There are quite a number of cell chemistry for Lithium (and possibly others).  Which one is good for Lora:Transmit time of 1.5 seconds or less, current 1C or less. Recharge 0.5C to be safe (may be 1C on spec.).Normal (non transmit) low duty cycle loa...
How to attach code in message so that it appears in grey box?   Many thanks
Which example 'may be' a better start for reading?  Do they use interrupt, DMA and power saving mode?SubGHz_Phy_PingPongLocalNetwork_Sensorhttps://github.com/STMicroelectronics/STM32CubeWL/tree/main/Projects/NUCLEO-WL55JC/Demonstrations/LocalNetwork/...