User Activity

Good day,  preparing to an online workshop I am trying to install prerequisites. However the component en.stedgeai-stneuralart-10.0.0.zip does not install, STM32CibeIDE says: "This file is either corrupted or not a recognized package.". Regards,Dmitr...
Dear All, On my NUCLEO-U575ZI-Q I have successfully generated USBX-DFU and have come to a point to connect to it with STM32CubeProgrammer. It seems to be very simple, there are six callbacks only:USBD_DFU_Activate and USBD_DFU_Deactivate does not ret...
Good day all, USBX crashes at line 171 of the file ux_dcd_stm32_initialize_complete.c, as the dcd structure is not initialized at this point. I have tried this on two different MCUs, U575 and H753. In concert, on the H753 the code generator does not ...
Hi all, I have just released subj. I have tried to contribute it to SQLite directly or to create a CubeMX package but seems that nobody interested, so I have created a standalone repository. I have used STM32H753I-EVAL2 to develop and test it and the...
Dear all, when I press Install button in the Toolchain Manager of the 1.17.0 CubeIDE it hangs after opening the subsequent dialog. I cannot close this dialog with neither mouse nor ESC key, need to terminate the task.  Regards,Dmitry