User Activity

Hi I m using F072 Nucleo bd, and compiler report the following errors but there was no syntax error from the code, can anyone advise?22:08:09 **** Incremental Build of configuration Debug for project F072_GPS_ NEO-6M_i2c_LCD_16x2 ****make -j8 allarm-...
Hi anyone know where to find this BOM and schematic diagram?
Hi i m currently coding standby mode to conserve battery energy a application, i know its the lowest current consumption, what and when to use the 3 modes? which mode should i use if i wana save battery life yet i still want SPI DMA to transfer in th...
hi I would like to know what does the f means in both 1000.0f and 2000.f ? anyone can kindly advise? ScalingFactor = 1000.0f/32768.0f; ScalingFactor = 2000.0f/32768.0f; 
hi come across these code using register programing, STM32F411 Nucleo bd, anyone can advise how does the (AF07<<4) and (AF07<<8) relate to UART2 PA2 & PA3? please advise..  #define AF07 0x07 GPIOA->AFR[1]|=(AF07<<4)|(AF07<<8); //ALT7 for UART2...