User Activity

Hello, I am developing an application, starting from stm32 empty project.The main file presents the following preprocessor header, that triggers the reported FPU initialization warning when I try to build the project.  #if !defined(__SOFT_FP__) && de...
Hello,I am using for the first time the FDCAN peripheral. I have configured it in classic CAN 2.0 mode and I have problems with transmission.In particular, when I start a transmission, nothing is output on the tx pin, and the TRP field in the FDCAN_T...
Hello,I am developing a CAN bus application.I am new to the FDCAN peripheral and I haven't understood the difference between nominal bit time parameters and data bit time parameters.Which of these two groups of parameters should I configure to obtain...
Hello,I need to implement delay macro, lasting just a few cycles.As the delay is so small I would not like to use TIMs o DWT.On Texas Instruments DSPs, I was used to implement this nanoseconds delays, using NOP() instructions.Unfortunately, as also w...
Hello,I have already seen some old post about this topic, but without a clear explanation and solution. I have the following function, to configure and enable timer with the desired period. void HW_TIMER_Enable(uint32_t period){  LL_TIM_SetAutoReload...