User Activity

Using STM32G030F6 and STM32CubeMX, I am trying to do a sequence of single channel conversions on each edge of a PWM signal (generated by an internal timer).  PWM is setup fine and working on TIM3 channel 1.   TIM3 TRGO is set to OC1REF.  ADC is set u...
I have been stuck on a tricky little issue for some time now.Using an STM32H753, on a reasonably large and complex application, when trying to erase the upper flash bank, the watchdog expires resetting the chip!My suspicion is that the CPU is stallin...
STM32Cube MX Version 6.1.1, STM32Cube MCU Package for STM32H7 Series V1.8.0eth.c is generated with the following code. It sets the MAC address assuming it is an array of bytes./* ETH init function */ void MX_ETH_Init(void) {   heth.Instance = ETH;...
I have been battling an issue for a while where upon a watchdog (WWDG1) timeout, the system was not correctly reset. I was finding that the CPU and NVIC are reset but all the peripherals are not reset after a watchdog reset, they keep their exact reg...
I have repeatedly observed that changing the watchdog prescaler on a running watchdog from 16 down to 4 usually causes the watchdog counter to eventually stop decrementing. I assume this happens due to something like decreasing the prescaler value b...
Kudos from