User Activity

New workspaceNew STM32 project Board Selector Nucleo-144 STM32H5 NUCLEO-H563ZITake the defaultsSet the tick to TIM6Pinout & Configuration - Middleware and Software Packs - THREADXGenerate App Init Code - checkSave everything, compile, debug, put a br...
The description of the ThreadX Application Queue Message Size in CubeIDE/CubeMX is vague.The queue size is specified in "words". The C language doesn't define how large a word is, it's not even processor implementation specific (I even read that Micr...
There are a bunch of CVEs for ThreadX, NetX, and USBX dealing with remote code execution in versions below 6.2.1 (with some pretty scary vulnerability scores) and fixed in 6.3.The distribution in the STM32Cube system is 6.2.0 today, and I was wonderi...
I have a project for STM32L452 using ThreadX and USBX, CubeIDE 1.14.1, firmware L4 1.18.0, on MacOS 14.3.1 Sonoma on Intel i9.In USBX/App/ux_device_descriptors.h I have placed some code:  /* Private defines -------------------------------------------...
I'm trying to get a L452 to bring up a VCP under ThreadX/USBx, so I followed the instructions in:https://community.st.com/t5/stm32-mcus/how-to-implement-the-usb-device-cdc-vcom-in-stm32-using-the/tac-p/629402#M738It seemed pretty straight forward, it...