User Activity

hi,I initialized string array with strings and type cast to uint32_t to store in flash memory as uint32_t. And then read the array as uint32_t. I update one of the string of the  array and type cast uint32_t to store that array in Flash memory back. ...
Hi,I wanted to send hexadecimal numbers through UART. I am using STM32F405. Can it be done.If I am sending float number as 1.3456 string (text) to windows COM port to  english language windows application field. If for example regional settings being...
Hi, I am having problem with string copy strncpy(). I am getting error message "Cannot access memory at address 0x31203a6e" static char *DataBuffer[30] = {0}; for(char *str =strtok((char*)recdata, "\n\n"); str; str = strtok(NULL, "\n\n")) { strncp...
Hi,I have question, I wanted to check whether a condition has reached below threshold level. How many check do I need to do whether it has reached the level below. Does it need to be three check or do a 20 check and average out to see if it below tha...
I am sending a command to the STM32F405 through the UART (COM) port for receiving data from the STM32F405. Once the command send from PC it will continously send data from STM32F405. What if the PC drops the connection and goes to sleep. And my STM32...