User Activity

Hi,I am trying to configure multiplexed OCTO SPI for the above MCU.Only Chip Select Port 1 NCS comes up as an alterantive for OCTOSPI1, and for OCTOSPI2 the Chip Select Port is is disabled, I would have expected Port 2 NCS to come up here... Is this ...
Hi,I am working with some custom boards for H7 and U5-series.The board schematics for STM32H735IG-DK and STM32U5A9-DISC shows both boards are using the same OCTO SPI but only the H7-board is using series resistors of 33 ohms for the all the data line...
Hi!At what speed would code in external flash memory execute? At the clock freq of the external flash or the by main clock freq of the MCU, or by some combination of the two?I assume once the code is fetched from the external flash, it would execute ...
Hi!The DEBUG build version of my custom loader is working but is slow, so I tried RELEASE build instead to hopefully get a smaller bin-file with a faster and more efficient execution.However, CubeProgrammer fails at startup with a “loading-file-error...
Hi!I am using a STM32U599VJT6 device without SMPS but getting this message when generating code:    What is supposed to be configured?Thanks in advance