User Activity

We are using the safety lib (-sl) command with X-CUBE-STL library. Without <pattern> parameter, it is working. When trying to use 0xFF for <pattern> parameter, generated .elf is not even valid and cannot be loaded. Is there a workaround for this?For ...
I have a question about X-CUBE-STL library on STM32H723ZG. We want to use it with a bootloader that resides in the first 128K flash sector. We want to reserve some data in the flash (firmware version and a signarure). Is there somewhere an example li...
I do not know if this is appropriate place to ask but I will try. We are integrating the STM STL library and we cannot get the flash test to be successful.This, this, this nor this helped. I believe we are generating the checksums correctly, we tried...
We are using custom board with STM32H735. We were debugging the same issue as this one. In the reference manual RM0468, we discovered this note:I think this means that even when not using calibration unit, FDCAN kernel clock must be <= than APB1 peri...
In LwIP examples for NUCLEO-H723ZG, in the linker, I think that there is an incorrect range of RAM_D2 memory.For example here: MEMORY { ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 12...
Kudos from