User Activity

Hi everybody, I'm trying to configure the Wi-Fi module on my custom board (based on the STM32MP153, the Wi-Fi module already tested OK) in Access point mode, and I found the official guide to set hostapd tool to do that: https://wiki.st.com/stm32mpu/...
Hi there, I may ask something **bleep** or impossible, but I want to try. Is there a way to debug (or at least look at the fault registers) a running MCU in a Fault state? In my case, I have an STM32H735g (so Cortex M7) which runs a FreeRTOS-based co...
Hi there, I'm developing a board that features the ST25R3911B chip. At the moment I managed to integrate the module in order to read and write simple NTAGs (t2t), with plain text (both on demoboard X-NUCLEO-NFC05A1 and my custom board).The next step ...
Hi there, I'm facing a problem with Cube IDE (ver. 1.13.0). Completely out of nowhere, it stopped letting me debug or run the code. When I click the buttons, I can see in the bottom right corner that it tries to launch the debugger, but it stops at L...
Hi everybody, I need to integrate the ST25R3911B NFC reader (X-NUCLEO-NFC05A1 a.t.m.) into a project with STM32H735G running FreeRTOS (with a TouchGFX task and another peripheral task running ). https://community.st.com/t5/st25-nfc-rfid-tags-and-read...