2015-11-10 5:56 AM
Hi All,
I am during writing bootloader for STLUX processor (base on STM8). Both, bootloader and main program uses own interrupt vector table. The STM8 processor has fixed interrupt vector table at 0x8000 address. I want to redirect from fixed vector table to vector table storing in RAM. I wrote the code to copy vector table from bootloader or main program to RAM and it is work fine, but I have problem with redirection. I do not know how can I do this. I use an IAR. I did an initialization a fixed vector table like this:typedef
void
(__far_func * interrupt_handler_t)(
void
);
struct
interrupt_vector {
unsigned
char
interrupt_instruction;
interrupt_handler_t interrupt_handler;
};
struct
interrupt_vector RamISR_IRQ[32] @ 0x00100;
struct
interrupt_vector
const
_vectab[] @ 0x8000
= {
{0x82, (interrupt_handler_t)(RamISR_IRQ)},
/* reset */
{0x82, (interrupt_handler_t)(RamISR_IRQ+ 1)},
/* trap */
{0x82, (interrupt_handler_t)(RamISR_IRQ+ 2)},
/* irq0 */
{0x82, (interrupt_handler_t)(RamISR_IRQ+ 3)},
/* irq1 */
{0x82, (interrupt_handler_t)(RamISR_IRQ+ 4)},
/* irq2 */
{0x82, (interrupt_handler_t)(RamISR_IRQ+ 5)},
/* irq3 */
{0x82, (interrupt_handler_t)(RamISR_IRQ+ 6)},
/* irq4 */
{0x82, (interrupt_handler_t)(RamISR_IRQ+ 7)},
/* irq5 */
{0x82, (interrupt_handler_t)(RamISR_IRQ+ 8)},
/* irq6 */
{0x82, (interrupt_handler_t)(RamISR_IRQ+ 9)},
/* irq7 */
{0x82, (interrupt_handler_t)(RamISR_IRQ+10)},
/* irq8 */
{0x82, (interrupt_handler_t)(RamISR_IRQ+11)},
/* irq9 */
{0x82, (interrupt_handler_t)(RamISR_IRQ+12)},
/* irq10 */
{0x82, (interrupt_handler_t)(RamISR_IRQ+13)},
/* irq11 */
{0x82, (interrupt_handler_t)(RamISR_IRQ+14)},
/* irq12 */
{0x82, (interrupt_handler_t)(RamISR_IRQ+15)},
/* irq13 */
{0x82, (interrupt_handler_t)(RamISR_IRQ+16)},
/* irq14 */
{0x82, (interrupt_handler_t)(RamISR_IRQ+17)},
/* irq15 */
{0x82, (interrupt_handler_t)(RamISR_IRQ+18)},
/* irq16 */
{0x82, (interrupt_handler_t)(RamISR_IRQ+19)},
/* irq17 */
{0x82, (interrupt_handler_t)(RamISR_IRQ+20)},
/* irq18 */
{0x82, (interrupt_handler_t)(RamISR_IRQ+21)},
/* irq19 */
{0x82, (interrupt_handler_t)(RamISR_IRQ+22)},
/* irq20 */
{0x82, (interrupt_handler_t)(RamISR_IRQ+23)},
/* irq21 */
{0x82, (interrupt_handler_t)(RamISR_IRQ+24)},
/* irq22 */
{0x82, (interrupt_handler_t)(RamISR_IRQ+25)},
/* irq23 */
{0x82, (interrupt_handler_t)(RamISR_IRQ+26)},
/* irq24 */
{0x82, (interrupt_handler_t)(RamISR_IRQ+27)},
/* irq25 */
{0x82, (interrupt_handler_t)(RamISR_IRQ+28)},
/* irq26 */
{0x82, (interrupt_handler_t)(RamISR_IRQ+29)},
/* irq27 */
{0x82, (interrupt_handler_t)(RamISR_IRQ+30)},
/* irq28 */
{0x82, (interrupt_handler_t)(RamISR_IRQ+31)},
/* irq29 */
};
The result:
As You see, The vector table from bootloader and ram is identical, so it is ok, but the values in fixed vector table are incorrect. I do not know why :(
Any idea? Update: When I manually set fixed vector table (0x8000 to 0x8080) to 0x00 (clear it, green color in above image) I see it is not programming by IDE (all bytes in section are still zero). Of course, I still uses a code attached above. *icf file://///////////////////////////////////////////////////////////////
// Example ILINK command file for
// STM8 IAR C/C++ Compiler and Assembler.
//
// Copyright 2014 IAR Systems AB.
//
/////////////////////////////////////////////////////////////////
define memory with size = 16M;
define region TinyData = [from 0x00 to 0xFF];
//define region RamVector = [from 0x00100 to 0x017F];
define region NearData = [from 0x00100 to 0x07FE];
define region Eeprom = [from 0x4000 to 0x43FF];
define region BootROM = [from 0x6000 to 0x67FF];
define region RedirectVector = [from 0x8000 to 0x8080];
define region BootloaderVector = [from 0x8080 to 0x8100];
define region NearFuncCode = [from 0x8080 to 0xFFFE];
define region FarFuncCode = [from 0x8080 to 0xFFFE];
define region HugeFuncCode = [from 0x8080 to 0xFFFE];
/////////////////////////////////////////////////////////////////
define block CSTACK with size = _CSTACK_SIZE {};
define block HEAP with size = _HEAP_SIZE {};
define block BOOTLOADERINTVEC with size = 0x80 { ro section .intvec };
define block REDIRECTINTVEC with size = 0x80 { ro section .rivector };
// Initialization
initialize by copy { rw section .far.bss,
rw section .far.data,
rw section .far_func.textrw,
rw section .huge.bss,
rw section .huge.data,
rw section .huge_func.textrw,
rw section .iar.dynexit,
rw section .near.bss,
rw section .near.data,
rw section .near_func.textrw,
rw section .tiny.bss,
rw section .tiny.data,
ro section .tiny.rodata };
initialize by copy with packing = none {section __DLIB_PERTHREAD };
do not initialize { rw section .eeprom.noinit,
rw section .far.noinit,
rw section .huge.noinit,
rw section .near.noinit,
rw section .tiny.noinit,
rw section .vregs };
// Placement
place at start of TinyData { rw section .vregs };
place in TinyData { rw section .tiny.bss,
rw section .tiny.data,
rw section .tiny.noinit,
rw section .tiny.rodata };
place at end of NearData { block CSTACK };
place in NearData { block HEAP,
rw section __DLIB_PERTHREAD,
rw section .far.bss,
rw section .far.data,
rw section .far.noinit,
rw section .far_func.textrw,
rw section .huge.bss,
rw section .huge.data,
rw section .huge.noinit,
rw section .huge_func.textrw,
rw section .iar.dynexit,
rw section .near.bss,
rw section .near.data,
rw section .near.noinit,
rw section .near_func.textrw };
place in BootloaderVector { block BOOTLOADERINTVEC };
place in RedirectVector { block REDIRECTINTVEC };
place in NearFuncCode { ro section __DLIB_PERTHREAD_init,
ro section .far.data_init,
ro section .far_func.textrw_init,
ro section .huge.data_init,
ro section .huge_func.textrw_init,
ro section .iar.init_table,
ro section .init_array,
ro section .near.data_init,
ro section .near.rodata,
ro section .near_func.text,
ro section .near_func.textrw_init,
ro section .tiny.data_init,
ro section .tiny.rodata_init };
place in FarFuncCode { ro section .far.rodata,
ro section .far_func.text };
place in HugeFuncCode { ro section .huge.rodata,
ro section .huge_func.text };
place in Eeprom { section .eeprom.noinit };
place in Eeprom { section .eeprom.data };
place in Eeprom { section .eeprom.rodata };
/////////////////////////////////////////////////////////////////
Thanks for any help.