cancel
Showing results for 
Search instead for 
Did you mean: 

I need the driver for the EVALKITST8500-1 evaluation kit (Windows 7)

Sameer Damir
Associate
Posted on December 08, 2017 at 11:26

I cant connect to my EVALKITST8500-1 using Smartgrid LabTool V4.4.

The power cable and the USB cable for kit interface are connected properly.

When I connect the interface cable as per the the quick start guide, the LabTool does not recognize any port.

If I go to settings - port: I can find no port to choose

If I go to settings - COM port - Scan port: Again, nothing happens.

In my windows device manager, I can see two new devices which don't have the appropriate driver, there are named: Enhanced COM port, and standard COM port.

#evalkitst8500-1 #smartgrid-labtool
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0