cancel
Showing results for 
Search instead for 
Did you mean: 

AWU Example

bruno2
Associate
Posted on May 26, 2014 at 20:53

Hi,

i´m having some problem with my code. I can´t use AWU.

Can anybody send me an example?
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
B.Montanari
ST Employee
Posted on May 29, 2014 at 23:05

Hi Bruno,

You can find one example code here: http://www.st.com/web/catalog/tools/FM147/CL1794/SC1807/SS1754/PF258009

Once downloaded, unzip the folder and go to this section: \STM8S_StdPeriph_Lib_V2.1.0\Project\STM8S_StdPeriph_Examples\AWU\AWU_ActiveHaltMode

There is also an app note: http://www.st.com/web/catalog/tools/FM147/CL1794/SC1807/SS1754/PF257990

Hope this will help you

B.Montanari
dvelasco
Associate II
Posted on June 06, 2014 at 22:47

I'm looking for the same kind of information.  I'm using an STM8L though, and the example code mentioned earlier is for the STM8S.  It doesn't seem to apply to the hardware that I'm using.

Help, please?  None of the sample code that I've found so far has been very helpful.