cancel
Showing results for 
Search instead for 
Did you mean: 

About Top level interrupt sensitivity

khal2 doe2
Associate
Posted on July 04, 2018 at 16:16

In this code,

I understand the line

''EXTI_SetExtIntSensitivity(EXTI_PORT_GPIOB , EXTI_SENSITIVITY_FALL_ONLY);''

It means EXTI detects falling edge, right?

But what's the next line means??

''EXTI_SetTLISensitivity(EXTI_TLISENSITIVITY_FALL_ONLY);'' 

0690X0000060LbtQAE.png

I read the reference manual about EXTI section but there is no enough information about TLIS..

0690X0000060LOlQAM.png
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
henry.dick
Senior II
Posted on July 04, 2018 at 18:41

the note you showed up says it clearly: it is the sensitivity for the TLI pin.

PZarc
Associate II

I understand, this pin PD7 cannot be acting with interrupt in the same time with PD0,PD1...6. Is it correct?