cancel
Showing results for 
Search instead for 
Did you mean: 

Error installing stm32cubeproj 2.12.0 SEVERE: com.izforge.izpack.api.exception.IzPackException: Console implementation not found for panel: com.st.CustomPanels.AnalyticsPanels

GJet7
Associate

WORKING:

> sudo java -jar SetupSTM32CubeProgrammer-2.11.0.exe

FAILS

> sudo java -jar SetupSTM32CubeProgrammer-2.12.0.exe

Completely uninstalled JAVA, then reinstalled - no change.

Reviewed several community posts, no solution yet.

Environment: macOS Big Sur

5 REPLIES 5
Zak
Associate II

Same issue on Feb 6th, 2023

Dfabr.1
Associate

Bonjour j'ai le même souci avec Debian.En utilisant l'ordonnanceur Linux et Windows.

manque t il une librairie en java?

MKori.1
Associate III

Same issue today under Linux with:

> sudo ./SetupSTM32CubeProgrammer-2.13.0.linux

jhnlmn
Associate III

It appears that SetupSTM32CubeProgrammer is a GUI app, so it has to be run without sudo but with DISPLAY:

DISPLAY=:0 ./SetupSTM32CubeProgrammer-2.14.0.linux

Yes! You are correct. This works for me also with Version 2.13. Very interesting information as I didn't find any information about a change in the installer in the release notes for 2.11.

Thank you!