cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer "Device memory - save as" - bug and more comfort to store option bytes in srec/hex/bin-file

STE_Michael
Associate II

Hello,
here are a few issues and requests for the STM32CubeProgrammer.

1. More comfort to store option bytes in srec/hex/bin-file
It is possible to store the option bytes configuration directly in a srec/hex/bin-File?
Currently, only export to a JSON file is possible.

2. If several ‘device memory’ tabs with different addresses are open, only the information from the first tab on the far left is saved when you select ‘Save as’ to save to a file. 

3. Why can't the STM32 CubeProgrammer be used in offline mode?
A programming interface and a microcontroller must always be connected.

The old STVP for the old STM8 was more practical in this respect.

Frustrated regards,
Michael









0 REPLIES 0