2025-09-18 4:54 PM
When I am trying to use the STM32CubeProgrammer in Linux, only the default connection option of J-Link is available. No other options "drop down" in the drop-down menu. Since I am set up to connect over USB, this means I am unable to connect to or reprogram the board (STM32MP257F-DK).
When I test this same thing on Windows, it shows USB as a connection option, and it can connect successfully. The drop-down menu appears normal. It used to work properly like this in Linux before, and I don't believe I changed any settings in STM32CubeProgrammer since then.
Is there a way I can get the standard behavior back when using Linux? I am following the steps as described here: https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP2_boards/STM32MP257x-DK/Let%27s_start/Populate_the_target_and_boot_the_image
Solved! Go to Solution.
2025-09-30 7:16 AM
Hello @rdmikkelsen
I'm seeing files with execute permissions that AFAIK should not be there. Could you try moving them somewhere else and retry. Maybe they're causing a conflict of some kind.
Aziz
2025-09-23 7:34 AM
Hello @rdmikkelsen
Please refer to STM32CubeProgrammer user manual page 13.
You need to install libusb via this command line:
sudo apt-get install libusb-1.0.0-dev
I also suggest copying the rules in "[CubeProgrammer install path]/Driver/rules" into "/etc/udev/rules.d" to have all interfaces available. You can navigate to it and use :
sudo cp *.* /etc/udev/rules.d
Hope you'll find this helpful.
Aziz
2025-09-23 10:36 AM
Thank you for the response. I can confirm that libusb was already installed as stated in the manual, and the udev rules were copied into that location. With the commands you gave, I got messages confirming that libusb was already on the newest version, and the relevant rules are already present in /etc/udev/rules.d
Is there anything else that could potentially cause issues here?
2025-09-25 2:34 AM
Hello,
Are you sure you restarted STM32CubeProgrammer after those modifications? Could you try running ls on /etc/udev/rules.d and share the output?
Thanks,
Aziz
2025-09-29 4:53 PM
2025-09-30 7:16 AM
Hello @rdmikkelsen
I'm seeing files with execute permissions that AFAIK should not be there. Could you try moving them somewhere else and retry. Maybe they're causing a conflict of some kind.
Aziz
2025-10-14 3:28 AM
Hello @rdmikkelsen
Any update after the last suggestion?
Aziz
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.