2024-11-29 12:15 AM - last edited on 2024-11-29 02:25 AM by SofLit
171192 is still ignoring...
Related to the thread: https://community.st.com/t5/stm32cubeprogrammer-mcus/dfu-mode-read-out-protection/m-p/683720
2024-11-29 02:05 AM
Hello @remov-b4-flight,
To provide more details on 171192. It comes from the non compatibility of the system bootloader with "Intel(R) USB 3.1 eXtensible Host Controller - 1.20 (Microsoft)"
=> Issue isn't a bug in the tool itself. With that being said, you have the following workarounds available:
1- Using a hub between PC and target
2- Rolling back to "Intel(R) USB 3.1 eXtensible Host Controller - 1.10 (Microsoft)"
3- Developing your own custom bootloader
STM32CubeProgrammer team is actively working on implementing a workaround to the issue inside the tool (Even though the issue isn't coming from the tool). I will keep you posted if I have any news
Aziz