cancel
Showing results for 
Search instead for 
Did you mean: 

STM32_Programmer_CLI.exe doesn't give result about the process.

carleslsregner
Associate III

carleslsregner_0-1767967136516.png

My goal is to use the STM32_Programmer_CLI.exe  from an application, but, for the moment, I just write down command lines in the Command Prompt (cmd.exe).

However, the commands of writting the flash ( -w yourbinfile.bin )and erasing it completely (-e all) does not return any kinf of results. I just delivers a "STM32CubeProgrammer v2.21.0" response. Why?

carleslsregner_1-1767967597947.png

 

 

 

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
Aziz BRIGUI
ST Employee

Hi @carleslsregner

You have to connect to the MCU first, if you're using ST-Link try:

STM32_Programmer_CLI -c port=SWD -w YourBinary.bin 0x08000000

Aziz 


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Aziz BRIGUI
ST Employee

Hi @carleslsregner

You have to connect to the MCU first, if you're using ST-Link try:

STM32_Programmer_CLI -c port=SWD -w YourBinary.bin 0x08000000

Aziz 


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

That's correct:

writting is impossible without connection and verification is impossible without writting.